5V Power supply - Microcontroller S912ZVCA19F0MKH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

5V Power supply - Microcontroller S912ZVCA19F0MKH

Jump to solution
1,353 Views
gpira
Contributor III

Hi, I would like to to power up the micro with a 5V power supply. I have seen from previous posts that to do so it is nesccesary to connect together all the bpower pins (VSUP, VDDC,VDDX,VDDA), but I was wondering if there is any official documentation on the issue, like an application note or similar.

Moreover, what I have to do with the ballast connections? Should I leave them floating?

Thanks in advance.

Best regards,

G. Pira

0 Kudos
Reply
1 Solution
1,342 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi G. Pira,

It is not officially supported and there is no such document.

The VSUP pin must not be left unconnected.

If you want to use an external 5V regulator, it must supply VSUP as well.

The MagniV series is design for 12V systems, it has internal LDOs and, for example, the BATS module that monitors the VSUP power supply.

Also, because the consumption of the CANPHY can be significant under certain conditions, the S12ZVC has a separate regulator for it.

Please have a look at Appendix I S12CANPHY Electrical Specifications in the S12ZVC RM.

If the ballast transistors are not used, the BCTL pins should be left unconnected.

AN4867, Hardware Design Guidelines for S12ZVC, Chapter 11 Unused pins.

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-m...

 

Regards,

Daniel

 

 

 

View solution in original post

1 Reply
1,343 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi G. Pira,

It is not officially supported and there is no such document.

The VSUP pin must not be left unconnected.

If you want to use an external 5V regulator, it must supply VSUP as well.

The MagniV series is design for 12V systems, it has internal LDOs and, for example, the BATS module that monitors the VSUP power supply.

Also, because the consumption of the CANPHY can be significant under certain conditions, the S12ZVC has a separate regulator for it.

Please have a look at Appendix I S12CANPHY Electrical Specifications in the S12ZVC RM.

If the ballast transistors are not used, the BCTL pins should be left unconnected.

AN4867, Hardware Design Guidelines for S12ZVC, Chapter 11 Unused pins.

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/s12-m...

 

Regards,

Daniel