320x240 TFT LCD App. - MC9S12X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

320x240 TFT LCD App. - MC9S12X

2,489 Views
abicash
Contributor III
Hi
I have an enquiry where I have to drive a 320x240 pix TFT-LCD screen (18bit RGB interface having 6bits/colour).I have to use a controller device which can drive this ,as well as do some controls with a hardware (real world) interface. This interface is digital so I would not worry about ADC.

I was suggested to have a look at MC9S08LC family for 8bit and in 16 bit ,to have a look at MC9S12X family.

Can anyone suggest something here? Any bit of information will be useful.

Awaiting reply as always I've had on this forum :smileyhappy:

Thanks and regards

 
 
Added p/n to subject.


Message Edited by NLFSJ on 2008-05-26 03:30 AM
Labels (1)
0 Kudos
Reply
1 Reply

693 Views
abicash
Contributor III
Hi :smileyhappy:

I have seen AN3493 where S12XE drives a 320x96 pixel TFT directly from XGATE.
Seems its the limit on S12XE.Can someone point out somewhere I can look for my application.
It seems that to drive this 320x240 from an XGATE , I will require an FPGA inbetween.

Thanks and regards

0 Kudos
Reply