basic thread connection is not getting established

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

basic thread connection is not getting established

2,782件の閲覧回数
shahprachi2427
Contributor I

i am not able to connect my iot toolbox application to the rapid iot kit do i need some other kind of hardware to connect because i have 3 rapid iot kit from none of them i m able to connect 

ラベル(1)
0 件の賞賛
返信
1 返信

2,672件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Prachi, I hope you're doing well!

 

The IOT Toolbox Mobile Application is looking for a specific UUID to connect to the device via Bluetooth. The example has to use this UUID so it doesn’t get filtered out from the IOT Toolbox Mobile Application Device list, and this UUID is the one used by the hybrid BLE-Thread Wireless UART for the KW41Z.

This is not implemented in the Out-Of-Box example for the Rapid IOT prototyping kit and requires a custom implementation.

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

0 件の賞賛
返信