basic thread connection is not getting established

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

basic thread connection is not getting established

2,747 Views
shahprachi2427
Contributor I

i am not able to connect my iot toolbox application to the rapid iot kit do i need some other kind of hardware to connect because i have 3 rapid iot kit from none of them i m able to connect 

Labels (1)
0 Kudos
Reply
1 Reply

2,637 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Prachi, I hope you're doing well!

 

The IOT Toolbox Mobile Application is looking for a specific UUID to connect to the device via Bluetooth. The example has to use this UUID so it doesn’t get filtered out from the IOT Toolbox Mobile Application Device list, and this UUID is the one used by the hybrid BLE-Thread Wireless UART for the KW41Z.

This is not implemented in the Out-Of-Box example for the Rapid IOT prototyping kit and requires a custom implementation.

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

0 Kudos
Reply