Thread Not runninng on Rapid IoT Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Thread Not runninng on Rapid IoT Kit

1,527 Views
ashokfair
Contributor IV

HI All,

I flashed (from KW41z SDK) hybrid example (thread router+ble) on Rapid IoT Kit. Aftr power on im able to connect with

IoT ToolBox App (thread Shell). Then I sent the command “thr create” and got success response, after I sent “thr join”

Thread joined , commission started  response received.

 

Now again I sent “thr join”  the expected response is “Already Connected”  but I received “Thread Joining…” then “commission started”

 

Once again if I send “thr join” same thing happening. Anyone have idea on this?

 

when we do scan from another router (FRDM board) I could see this Rapid IoT kit on the list.

Note: I'm not using the default application example which comes with Rapid IoT Kit with FSCI communication. In my case K64F is flashed with hello world.

Labels (1)
0 Kudos
Reply
4 Replies

1,351 Views
trialaccount12
Contributor V

Hi,

   I also have a similar question. Did you flash "thread example" project from KW41z SDK onto rapid Iot board? Or could you share the SDK here? I was partly successful in this approach.

Regards

Niranjan

0 Kudos
Reply

1,351 Views
ashokfair
Contributor IV

Yes, i flashed from KW41z SDK examples. The SDK you can download from NXP SDK Builder https://mcuxpresso.nxp.com/en/builder  SDk 2.2.0

0 Kudos
Reply

1,351 Views
trialaccount12
Contributor V

Yes, I too tried the same. I was able to create a thread network but for some reason i was not able to get any response from other board.

Regards

Niranjan

0 Kudos
Reply

1,351 Views
ashokfair
Contributor IV

Th reason is K64F firmware, try to flash kboot in K64 and check..  still i m finding proper way of initialization to

get rid of this issue.