DPS in Azure SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DPS in Azure SDK

2,091件の閲覧回数
pritesh_shah
Contributor I

Hello,

I need to provision the kinetis k64 based device with the Azure portal. so
I have downloaded an SDK for Kinetis K64.

I have seen the example to connect the device with the Azure cloud.
But I did not find support for auto-provisioning of the device with Azure cloud.
SDK does not include support for Device Provisioning Service.

Please guide me on how I can achieve the zero-touch provisioning with Azure cloud
and provide the sample example for that.

タグ(2)
0 件の賞賛
返信
1 返信

1,975件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Pritesh,

Hope you are doing well.

Any implementation of different features must be done by our customers. We do not have examples using the K64 for zero touch provisioning. I recommend that you check the following documentation that will help you as a reference on how to get started. 

Overview of Azure IoT Hub Device Provisioning Service | Microsoft Docs 

Set up IoT Hub Device Provisioning Service in the Azure portal | Microsoft Docs 

https://community.nxp.com/docs/DOC-329718 

Hope it helps!

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信