{standard input}:361: Error: unrecognized opcode: `rorw'

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

{standard input}:361: Error: unrecognized opcode: `rorw'

1,446件の閲覧回数
1475849560
Contributor II

I compiled BusyBox using E500v2 SDK2.0 and found this problem

rowo.png

4J~JQ8UKZYP6M~1T})XYUG5.png

0 件の賞賛
返信
1 返信

1,436件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please install SOURCE ISO QorIQ-SDK-V2.0-SOURCE-20160527-yocto.iso and Cache ISO QorIQ-SDK-V2.0-PPCE500V2-CACHE-20160527-yocto.iso in the same path.

Then execute the following command to create the build project.

$ source ./fsl-setup-env -m c293pcie

Then execute "bitbake busybox", you will find busybox images in QorIQ-SDK-V2.0-20160527-yocto/build_c293pcie/tmp/work/ppce500v2-fsl-linux-gnuspe/busybox/images.

0 件の賞賛
返信