qemu-system-ppc64 vhost-net support is not compiled in

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

qemu-system-ppc64 vhost-net support is not compiled in

6,531件の閲覧回数
abhinavbipnesh
Contributor I

Hi,

While trying to bring ethernet interface using tap0 I am getting below errors

qemu-system-ppc64: -netdev tap,id=tap0,script=no,vhost=on: vhost-net support is not compiled in

qemu-system-ppc64: -netdev tap,id=tap0,script=no,vhost=on: vhost-net requested but could not be initialized

qemu-system-ppc64: -netdev tap,id=tap0,script=no,vhost=on: Device 'tap' could not be initialized

The command which I tried to fire is given below

sudo ~/QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/sysroots/x86_64-linux/usr/bin/qemu-system-ppc64 -cpu e5500 -nographic -m 256 -M ppce500 -kernel uImage -initrd fsl-image-minimal-t1040rdb-20141223093206.rootfs.ext2.gz -append "root=/dev/ram rw console=ttyS0,115200" -serial tcp::4444,server,telnet -netdev tap,id=tap0,script=no,vhost=on -device virtio-net-pci,netdev=tap0

The system configuration is given below

Build Configuration:

BB_VERSION        = "1.22.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "CentOS-7.0.1406"

TARGET_SYS        = "powerpc-fsl-linux"

MACHINE           = "t1040rdb"

DISTRO            = "fsl-networking"

DISTRO_VERSION    = "1.6"

TUNE_FEATURES     = "m32 fpu-hard e5500"

TARGET_FPU        = "hard"

meta

meta-yocto

meta-yocto-bsp    = "(detachedfromfsl-sdk-v1.6):0d2ce44c2b0f8cc9699e30cca2c24655be89d58b"

meta-fsl-ppc      = "(detachedfromfsl-sdk-v1.6):6cf59d9de63a9fc5f8942c0d10c622898f4315ce"

meta-fsl-ppc-toolchain = "(detachedfromfsl-sdk-v1.6):a546e42f86e7d57de19e27907365d170b13fc18f"

meta-fsl-networking

meta-fsl-networking = "(detachedfrom8dec9c6):8dec9c690188cce5305ef5055f91e5cfa35c63f4"

meta-virtualization

meta-virtualization = "(detachedfromfsl-sdk-v1.6):8044073f63a0d99541a43ac5f2f6d789f94c7c7c"

meta-oe

meta-networking

meta-webserver

meta-ruby

meta-filesystems  = "(detachedfromfsl-sdk-v1.6):b86007f742a1b829ccc8d76e485bb3f789cefaa4"

meta-java         = "(detachedfromfsl-sdk-v1.6):d01f7d39e513790ddce20e6724723722119a3700"

meta-openstack

meta-openstack-compute-deploy

meta-openstack-controller-deploy

meta-openstack-qemu = "(detachedfromfsl-sdk-v1.6):f627404399a134672e0b5e26a0d9b794a6f8adf4"

So any thoughts how to fix it as I tried even recompling the Kernel as given part of  http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F2888263.html but still I am getting same error.

Thanks,

Abhinav

タグ(2)
0 件の賞賛
返信
7 返答(返信)

5,327件の閲覧回数
abhinavbipnesh
Contributor I

Finally I am able to solve the issue. Basically I need to create tap0 device manually using below steps. Below are the instruction for CentOs 7. So hopefully same or modified steps can work on other OS.

1. Create a TAP device using below steps. Setting its IP address as 192.168.7.1 (other whatever you want to set it.) The main thing is to set the Gateway as 192.x.x.1 as it will act as gateway device for the QEMU machine.

  1. # ip tuntap add tap0 mode tap
  2. # ifconfig tap0 192.168.7.1 netmask 255.255.255.0
  3. Now using sample scripts of openvpn create a bridge interface with physical interface. Follow the instruction given in this link(no need to configure server side scripts as they are not used) . https://openvpn.net/index.php/open-source/documentation/miscellaneous/76-ethernet-bridging.html
  4. Now fire the QEMU interface command to start the machine. Now this machine can talk to outside world using TAP interface.

Hope this will help if some one is looking for interfacing stuff.

-Abhinav


0 件の賞賛
返信

5,327件の閲覧回数
scottwood
NXP Employee
NXP Employee

Again, you appear to be running QEMU on an x86 host (based on "sysroots/x86_64-linux" -- if that is not the case, and you're actually trying to run this on the PPC board, please let me know as Yocto is not my area of expertise).  vhost_net is for KVM.  You can't use KVM when the CPU types don't match.

0 件の賞賛
返信

5,327件の閲覧回数
abhinavbipnesh
Contributor I

Hi,

Basically I am trying to emulate PPC64e5500 as will be using T1024QorIQ (t1040rdb is the emulation board) on CentOs7 host. This build host or my development environment is on x86_64 with CentOs7 running on it.

The current SDK version which I am using is QorIQ-SDK-V1.6-PPC64E5500-IMAGE-20140619-yocto.iso for the same.

Now while trying to bring a QEMU based emulation we need to use physical ethernet interface i.e. eth0 for making this machine to talk to outside world. So I was trying to use TUN/TAP interface support which I think qemu-system-ppc is capable of doing so. So while passing the arguments to the commands I get this error. Even I tried to bring up the bridge interface using bridge-helper utility (part of the qemu-system-ppc) but similar error pops up.

Please let me know if you need more information.

Thanks,

Abhinav

0 件の賞賛
返信

5,327件の閲覧回数
abhinavbipnesh
Contributor I

Hi,

Below is the output from the QEMU machine

QEMU Machine

root@model:~# cat /proc/cpuinfo

processor       : 0

cpu             : e5500

clock           : 400.000000MHz

revision        : 2.0 (pvr 8024 1020)

bogomips        : 800.00

total bogomips  : 800.00

timebase        : 400000000

platform        : QEMU e500

model           : QEMU ppce500

Memory          : 128 MB

Host Machine

[root@mydevbox2 ~]# cat /etc/redhat-release

CentOS Linux release 7.0.1406 (Core)

[root@mydevbox2 ~]# uname -an

Linux mydevbox2 3.10.0-123.13.1.el7.x86_64 #1 SMP Tue Dec 9 23:06:09 UTC 2014 x86_64 x86_64 x86_64 GNU/Linux

Command to bring up the QEMU machine

sudo ~/QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/sysroots/x86_64-linux/usr/bin/qemu-system-ppc64 -cpu e5500 -nographic -m 256 -M ppce500 -kernel uImage -initrd fsl-image-minimal-t1040rdb-20141223093206.rootfs.ext2.gz -append "root=/dev/ram rw console=ttyS0,115200 ip=192.168.7.2::192.168.7.1:255.255.255.0 mem=128M" -serial tcp::4444,server,telnet -net nic,model=e1000 -net tap,ifname=tap0,script=no,downscript=no

QEMU 1.7.0 monitor - type 'help' for more information

(qemu) QEMU waiting for connection on: telnet:0.0.0.0:4444,server

Also observed an bug with the qemu-bridge-helper script as it look for bridge.conf at a hard coded path as same can be verified as below

sudo ~/QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/sysroots/x86_64-linux/usr/bin/qemu-system-ppc64 -cpu e5500 -nographic -m 256 -M ppce500 -kernel uImage -initrd fsl-image-minimal-t1040rdb-20141223093206.rootfs.ext2.gz -append "root=/dev/ram rw console=ttyS0,115200 ip=192.168.7.2::192.168.7.1:255.255.255.0 mem=128M" -serial tcp::4444,server,telnet -net nic -net tap,"helper=/home/abhinav/QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/sysroots/x86_64-linux/usr/lib/qemu/qemu-bridge-helper"

[sudo] password for abhinav:

failed to parse default acl file `/local/workspace/yocto-iso-make/sdk-v1.6.x/t1040rdb-64b/build_t1040rdb-64b_release/tmp/sysroots/x86_64-linux/etc/qemu/bridge.conf'

failed to launch bridge helper

qemu-system-ppc64: -net tap,helper=/home/abhinav/QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/sysroots/x86_64-linux/usr/lib/qemu/qemu-bridge-helper: Device 'tap' could not be initialized

So when I created a soft links for the files even the bridge-helper didn't bring the ethernet interface as the bridge is configured on my base machine.

>sudo ~/QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/sysroots/x86_64-linux/usr/bin/qemu-system-ppc64 -cpu e5500 -nographic -m 256 -M ppce500 -kernel uImage -initrd fsl-image-minimal-t1040rdb-20141223093206.rootfs.ext2.gz -append "root=/dev/ram rw console=ttyS0,115200 ip=192.168.7.2::192.168.7.1:255.255.255.0 mem=128M" -serial tcp::4444,server,telnet -net nic -net tap,"helper=/home/abhinav/QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/sysroots/x86_64-linux/usr/lib/qemu/qemu-bridge-helper"

failed to create tun device: Operation not permitted

failed to launch bridge helper

qemu-system-ppc64: -net tap,helper=/home/abhinav/QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/sysroots/x86_64-linux/usr/lib/qemu/qemu-bridge-helper: Device 'tap' could not be initialized

So any thoughts to bring up the interface will be a great help.

Please let me know if you need more information.

Thanks,

Abhinav

0 件の賞賛
返信

5,327件の閲覧回数
scottwood
NXP Employee
NXP Employee

Does your host kernel have CONFIG_TUN enabled (or the module loaded)?

0 件の賞賛
返信

5,327件の閲覧回数
abhinavbipnesh
Contributor I

Hi,

Please find below output of ipconfig as I am using openvpn for setting up tap device.

>ifconfig

br0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500

        inet 192.168.7.200  netmask 255.255.255.0  broadcast 192.168.7.255

        inet6 fe80::ec5b:17ff:fe7d:2c13  prefixlen 64  scopeid 0x20<link>

        ether 00:50:56:80:74:64  txqueuelen 0  (Ethernet)

        RX packets 3671  bytes 181803 (177.5 KiB)

        RX errors 0  dropped 0  overruns 0  frame 0

        TX packets 41  bytes 5155 (5.0 KiB)

        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

eno33557248: flags=4419<UP,BROADCAST,RUNNING,PROMISC,MULTICAST>  mtu 1500

        inet6 fe80::250:56ff:fe80:7464  prefixlen 64  scopeid 0x20<link>

        ether 00:50:56:80:74:64  txqueuelen 1000  (Ethernet)

        RX packets 34958  bytes 2137667 (2.0 MiB)

        RX errors 0  dropped 12  overruns 0  frame 0

        TX packets 981  bytes 69175 (67.5 KiB)

        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

tap0: flags=4355<UP,BROADCAST,PROMISC,MULTICAST>  mtu 1500

        inet6 fe80::9822:63ff:fe67:33eb  prefixlen 64  scopeid 0x20<link>

        ether 9a:22:63:67:33:eb  txqueuelen 100  (Ethernet)

        RX packets 42  bytes 3388 (3.3 KiB)

        RX errors 0  dropped 0  overruns 0  frame 0

        TX packets 3015  bytes 186074 (181.7 KiB)

        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

>ls -l /dev/net/tun

crw-rw-rw-. 1 root root 10, 200 Dec 24 17:14 /dev/net/tun

So it seems that tap device is up and running without any issue. Please let me know if you need more information.

Thanks,

Abhinav

0 件の賞賛
返信

5,327件の閲覧回数
scottwood
NXP Employee
NXP Employee

Note that you should be able to use ordinary virtio (not vhost) with QEMU regardless of KVM.

0 件の賞賛
返信