p1022 power on reset problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

p1022 power on reset problem

1,221 次查看
zeevg
Contributor I

Hi,

I working to bring up new board.

I see problem booting from parallel nor.

When making the reset via the ICE the booting is started.

when booting after power up or using reset switch (connected to the input of supervisory) the booting sometime not started.

I drive The CPU HRESET pin from supervisory (which guaranty clean and long signal) to AND gate which inputs are the ICE_Hreset and POReset.

In addition AND gate which inputs are the ICE_TRST and POReset drive the CPU TRST pin.

Pls. advise

Zeev Gerber

标记 (1)
0 项奖励
回复
1 回复

1,150 次查看
ufedor
NXP Employee
NXP Employee

It is needed to check the processor connection schematics as a whole.

Please create a Technical Case and provide the schematics:

https://community.freescale.com/thread/381898

0 项奖励
回复