p1022 cpu up timeout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

p1022 cpu up timeout

2,236件の閲覧回数
rinkutakkar
Contributor I

We are using P1022 in our design. In one of the boards core 1 does not boot up and following print is being displayed :-

"CPU up timeout. CPU up mask is 1 should be 3".

Please guide about the possible reasons for the same.

0 件の賞賛
返信
3 返答(返信)

2,146件の閲覧回数
ufedor
NXP Employee
NXP Employee

The issue corresponds to incorrect processor powering.

It is required to doublecheck the design referring the processor's Hardware Specifications and Design Checklist.

0 件の賞賛
返信

2,147件の閲覧回数
rinkutakkar
Contributor I

Thanks for your comments.

We have now configured this as P1013 by keeping the test_sel pin low and it is working properly.

We have checked all the power and clock rails and POR settings and they are as per processor specifications.

Kindly guide

0 件の賞賛
返信

2,147件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please create a Technical Case - reference:

https://community.freescale.com/thread/381898 

0 件の賞賛
返信