p1010 gianfar driver problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

p1010 gianfar driver problem

504件の閲覧回数
袁增兴
Contributor I

We use linux-3.10.59 from kernel.org for p1010

When we test eth throughput use smartbits, the console died,we can not input any thing to console or nothing print from console!

0 件の賞賛
返信
1 返信

450件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello zengxing yuan,

You could use SDK 1.9(Kernel 3.12) pre_bult images to do verification, SDK 1.9 pre-built image ISO can be downloaded from https://nxp.flexnetoperations.com/control/frse/product?child_plneID=684021&cert_num=181474981&ver=AR... 

You also could download Linux Kernel 4.x(4.1 or 4.4) from the upstream to build uImage to do verification,probably some patches are missed in the Kernel source which you downloaded.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信