mpic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mpic

2,373件の閲覧回数
hv
Contributor II

I'm using uboot on a T1040RDB.  I'm not sure about the mode of operation for MPIC.  How can I find out if uboot set up MPIC to be in external proxy, mixed or pass-through mode?  Thanks!

0 件の賞賛
返信
2 返答(返信)

2,266件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

MPIC supports several these modes, but actually only "mixed" mode is typically used. The only this mode allows using normal interrupt delivery and interrupt priority mechanisms described in T1040 Reference Manual, Section 25.4.1 "Flow of interrupt control".

In our T1040RDB we use mixed mode.

T1040 Reference Manual is available for download from T1040 product page, "Documentation" tab:

QorIQ® T1040 and T1020 Multicore Communications Processors|NXP 


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,266件の閲覧回数
hv
Contributor II

Thanks!

0 件の賞賛
返信