mpc8349ea mds bsp for linux - gdb

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mpc8349ea mds bsp for linux - gdb

跳至解决方案
5,522 次查看
rans
Senior Contributor I

Hello,

I have downloaded mpc8349ea  BSP, and wanted to use the binary for gdb in host & gdbserver in target.

Can anyone please point to where is can't be found ?

I have some issue installing the bsp with ltib and rpm version.

Regards,

Ran

0 项奖励
回复
1 解答
5,020 次查看
rans
Senior Contributor I

Hi Platon,

Is there any idea how I can resolve it ?

Thanks,

Ran

在原帖中查看解决方案

0 项奖励
回复
9 回复数
5,020 次查看
bpe
NXP Employee
NXP Employee

LTIB do have problems with newer Ubuntu releases. The last officially supported Ubuntu version is 8.10. There is a number of  posts in the community

where people share solutions:

ubuntu-ltib-patch.tgz

Re: LTIB on Ubuntu 12.04

Re: LTIB build fails on lkc, using Ubuntu 11.10 and LTIB 9.1.1

None of these, however, has been officially approved or supported.

As of GDB, yes, the bsp you are working with does include GDB.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
5,020 次查看
rans
Senior Contributor I

Hi,

Continuing effort, but no success yet.

After install of ubuntu 8.10, and other dependencies.

Now I get the following failure:

bison -y -d ./parse.y

make: *** [parse.c] Segmentation fault

Any ideas?

Regrads,

Ran

0 项奖励
回复
5,020 次查看
rans
Senior Contributor I

Hi Platon,

Thank you very much for your assistance!

I've tried to apply the patch in your first link (ubuntu-ltib-patch.tgz ) . I hope it will be OK for ubuntu 10.04 (The message menion only ubuntu 10.04).

What should I put in ltibDir ?

I have not installed any ltib in ubuntu ?

ubuntu@ubuntu-laptop:~/dtu/bsp/ubuntu-ltib-patch$ ./install-patches.sh ../ltib-mpc8349emds-20061221/

cp lkc-1.4-lib.patch /opt/freescale/pkgs

cp lkc-1.4-lib.patch.md5 /opt/freescale/pkgs

cp sparse-0.4-fixlabel.patch /opt/freescale/pkgs

cp sparse-0.4-fixlabel.patch.md5 /opt/freescale/pkgs

Patching Spec Files

cp: cannot stat `../ltib-mpc8349emds-20061221//dist/lfs-5.1/sparse/sparse.spec': No such file or directory

cp: cannot create regular file `../ltib-mpc8349emds-20061221//dist/lfs-5.1/sparse/sparse.spec': No such file or directory

cp: cannot stat `../ltib-mpc8349emds-20061221//dist/lfs-5.1/mux_server/mux_server.spec': No such file or directory

cp: cannot create regular file `../ltib-mpc8349emds-20061221//dist/lfs-5.1/mux_server/mux_server.spec': No such file or directory

Done

patching file bin/Ltibutils.pm

Hunk #1 FAILED at 584.

1 out of 1 hunk FAILED -- saving rejects to file bin/Ltibutils.pm.rej

I don't have any "mux_server.spec" in ubuntu folders.

Regards,

Ran

0 项奖励
回复
5,020 次查看
rans
Senior Contributor I

Hi Platon,

This is quite a trouble. I've had no luck with this issue.

I went back to install ubuntu 8.10.

But it get me just a little step to the next never-ending issues.

Is it possible to attach in this thread the gdb & gdbserver , just for me to try it in my environment ?

I already have everthing in my existing bsp, only the gdb&gdbserver are missing...

Best Regards,

Ran

0 项奖励
回复
5,020 次查看
bpe
NXP Employee
NXP Employee

The details you provided are not sufficient for any suggestion, sorry. Please update this thread with the following:

(a) The exact name of the BSP .iso image you are working with;

(b) Errors returned by LTIB

Note. Not all Freescale BSPs/SDKs include support to gdb.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
5,020 次查看
rans
Senior Contributor I

Thank you,

This issue been resolved.

I am working with compiled gdb / gdbserver it seems to work just fine.

I am not using freescale BSP from website, but buildroot with linux 3.14.25.

Regards,

Ran

0 项奖励
回复
5,020 次查看
rans
Senior Contributor I

Hi Platon,

As to the gdb issue, Do you know if there is any gdb & gdbsever available ? I've been really struglling at this without results so far.

Maybe there is someone who used it and can share ?

Thank you!

Ran

0 项奖励
回复
5,021 次查看
rans
Senior Contributor I

Hi Platon,

Is there any idea how I can resolve it ?

Thanks,

Ran

0 项奖励
回复
5,020 次查看
rans
Senior Contributor I

Hi,

Sorry, my apology.

1. The BSP is MPC8349EA_MDS_K26_20061221-LTIB.iso (this is the only image I found in the site, if there is any alternative to LTIB , it can be a good solution)

I am working on ubuntu 10.04 (virtualbox).

2. The errors I get:

ubuntu@ubuntu-laptop:~/dtu/dtu_src/dtu/src/modules/ltib-mpc8349emds-20061221$ ./ltib

ltib cannot be run because one or more of the host packages needed

to run it are either missing or out of date.

Please install/upgrade these packages and then re-try.

Package                Minimum ver   Installed info

-------                -----------   ---------------

rpm-build              0             not installed

Died at ./ltib line 1411.

Started: Wed Aug 12 14:52:58 2015

Ended:   Wed Aug 12 14:52:58 2015

Elapsed: 0 seconds

Build Failed

Exiting on error or interrupt

3. I tried to install rpm older version 4.4.3.2 , and it also failed in many depeneded ways, till I gave up with it.

Best Regards,

Ran

0 项奖励
回复