mpc8309 pci endpoint configure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mpc8309 pci endpoint configure

1,347件の閲覧回数
威杨
Contributor III

I  use mpc8309 as pci ep device under uboot, i configure  pci_ctrl->pitar0 = 0x7F00000,pci_ctrl->pibar0 = 0x80000000,pci_ctrl->piwar0 = 0x80055013, when pci root device write and read correspond endpoint ddr 0 address, not 0x7f00000,i need your help. 

THANKS.

ラベル(1)
0 件の賞賛
返信
1 返信

1,181件の閲覧回数
Pavel
NXP Employee
NXP Employee

Check the PCI Local Access Window Register (PCILAWBAR0) and PCI Local Access Window Attributes Register (PCILAWAR) settings. See attached files.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信