LS1043A, Reset configuration word (RCW) source Query

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A, Reset configuration word (RCW) source Query

3,342件の閲覧回数
logeshs
Contributor II

Hi

In LS1043A, we are using NOR as the Boot Memory. To chose NOR as the RCW source in boot strap setting we need to set as mentioned in the 4.4.5.1 Reset configuration word (RCW) source of reference Manual. As per our configuration say suppose cfg_rcw_src bits are : 0_0001_0101. Please confim which is the LSB bit in the binary sequence.

Thanks

0 件の賞賛
返信
1 返信

2,442件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

The cfg_rcw_src[0:8] are multiplexed on the IFC_AD[8:15], IFC_CLE pins. In the manual values the least significant bit corresponds to the cfg_rcw_src[8]. For cfg_rcw_ = 0_0001_0101, on power-on reset the IFC_AD[8] pin has to be pulled down while the IFC_CLE pin has to be pulled up (the LS bit is ‘1’).

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信