microcodes for DPAA and QUICC engine

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

microcodes for DPAA and QUICC engine

2,322件の閲覧回数
sivadattudwara
Contributor II

Hi,

     we are developing a bareboard software for T1024 processor. to develope drivers for DPAA and QUICC engine, can we use the microcodes provided by U-Boot as is? or do we need to change them as per our requirement? if we need to change them, how can we generate the new micro code for them? where i can get more information about these micro code?

3 返答(返信)

2,128件の閲覧回数
ufedor
NXP Employee
NXP Employee

> do we need to change them as per our requirement?

The microcodes have to be used "as is" - they are not intended to be modified by end-customers, so additional information of the microcodes internals is not provided.

2,128件の閲覧回数
sivadattudwara
Contributor II

Hi,

     Thanks for reply, want to know what is exact purpose of this microcode. will it initialize the complete hardware?  or do user has to perform some more initialization in drivers after uploading the microcode?

0 件の賞賛
返信

2,129件の閲覧回数
ufedor
NXP Employee
NXP Employee

Microcodes are required for hardware - FMan and QE.

Software drivers are also required and normally bundled with the operation system.

Linux SDK with required drivers is provided by NXP free of charge.