microcodes for DPAA and QUICC engine

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

microcodes for DPAA and QUICC engine

1,622 次查看
sivadattudwara
Contributor II

Hi,

     we are developing a bareboard software for T1024 processor. to develope drivers for DPAA and QUICC engine, can we use the microcodes provided by U-Boot as is? or do we need to change them as per our requirement? if we need to change them, how can we generate the new micro code for them? where i can get more information about these micro code?

3 回复数

1,428 次查看
ufedor
NXP Employee
NXP Employee

> do we need to change them as per our requirement?

The microcodes have to be used "as is" - they are not intended to be modified by end-customers, so additional information of the microcodes internals is not provided.

1,428 次查看
sivadattudwara
Contributor II

Hi,

     Thanks for reply, want to know what is exact purpose of this microcode. will it initialize the complete hardware?  or do user has to perform some more initialization in drivers after uploading the microcode?

0 项奖励
回复

1,429 次查看
ufedor
NXP Employee
NXP Employee

Microcodes are required for hardware - FMan and QE.

Software drivers are also required and normally bundled with the operation system.

Linux SDK with required drivers is provided by NXP free of charge.