ls1021a Hardcoded Option Codewarrior Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1021a Hardcoded Option Codewarrior Error

2,276件の閲覧回数
jiye
Contributor V

Hi,

I am trying to follow the reference manual 4.4.6.2 to create my 0x9A hard coded RCW settings for my ls1021a stand alone board. After I follow the recommended settings and regenerate the code it shows me an error below:

pastedImage_1.png

Can anyone help?

タグ(3)
0 件の賞賛
返信
5 返答(返信)

2,147件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Elias Bitbaker,

I didn't reproduce your project, please refer to my attached workspace.

0 件の賞賛
返信

2,147件の閲覧回数
jiye
Contributor V

your work space i load your PBL.bin file but it shows

pastedImage_1.png

IFC NAND (NAND flash) shouldn't it be eMMC

pastedImage_2.png

also if I want to use 0x9a hard coded option the clock should be 100 MHz right ?

pastedImage_3.png

0 件の賞賛
返信

2,147件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

On my side, the system clock frequency is 100MHz, please import the project form File->Import->General->Existing Projects into Workspace.

0 件の賞賛
返信

2,147件の閲覧回数
jiye
Contributor V

i did what you told me to do.

First of all can you answer this question would be super helpful

pastedImage_1.png

Do i need to change the RCW source to eMMC, hardcoded instead of IFC NAND????????? because I am flashing into the eMMC my customized board does not have NAND flash

I assume you was using 9A,  this what I did.

(1)I imported your project

(2) I went to generated code then I changed the pbl.bin to ls1021a-rcw.txt then I load this file from the debug configuration of my OCRAM board project

(3) I used OCRAM init script and memory script then run debug

0 件の賞賛
返信

2,147件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

No need to change RCW source.

0 件の賞賛
返信