golang

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

golang

2,726 Views
mlweber1
Contributor I

At one point there was basic support for 64bit big-endian e5500 and e6500 in GOlang but it was completely removed in the last year (I've still got to check if gccgo support is functional Crosscompiling go with C library on powerpc64 – dutkowski.me  ).  This pretty much means no use of any newer Linux container management tools. Or for that matter any GO based applications/libs.  Is there any internal NXP support for bringing back GOlang support for the QoriQ arch's?   Looks like a POWER8 standard is now the minimum for 64bit big-endian(all: require POWER8 support for ppc64, to match ppc64le · Issue #19074 · golang/go · GitHub ).

GOlang discussion about deprecation policy.

all: define deprecation policy for old architectures · Issue #19075 · golang/go · GitHub 

Discussion about dropping support.

cmd/link: ppc64 (big endian) cgo errors · Issue #13192 · golang/go · GitHub 

0 Kudos
Reply
2 Replies

2,266 Views
robertoinnocent
Contributor III

Hi we are very interested to make golang to be compiled on PPC64 Big Endian, why not make a task force of volunteer doing that?

0 Kudos
Reply

2,497 Views
ufedor
NXP Employee
NXP Employee

> Is there any internal NXP support for bringing back GOlang support for the QoriQ arch's?

There is no internal NXP project to provide requested support for QorIQ Power Architecture processors.

0 Kudos
Reply