fsl-image-kernelitb Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fsl-image-kernelitb Error

6,824件の閲覧回数
mounikareddy22
Contributor I

Hi,

I'm using yocto SDK 2.0, In which i'm trying to build Linux image for T4240RDB.

Following is the procedure followed:

1. bitbake -c menuconfig virtual/kernel
2. bitbake -c compile -f virtual/kernel
3. bitbake virtual/kernel
4. bitbake fsl-image-kernelitb

When i give "bitbake fsl-image-kernelitb",

"ERROR: Nothing PROVIDES 'fsl-image-kernelitb'
ERROR: fsl-image-kernelitb was skipped: incompatible with machine t4240rdb-64b (not in COMPATIBLE_MACHINE)" is displayed.

Could you please help me to proceed further.

Waiting for your reply..!

Thanks & Regards,

Mounika Reddy

タグ(1)
0 件の賞賛
返信
3 返答(返信)

5,431件の閲覧回数
Pavel
NXP Employee
NXP Employee

The T4240 u-boot does not supports .itb files. There is no the fsl-image-kernelitb.bbappend for the T4240.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,431件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP SDK 2.0 does not support kernelitb for the T4240. This option is available for the LS1012a. LS1043a and LS1046a. See the following file:

QorIQ-SDK-V2.0-20160527-yocto/sources/meta-nxp-npi-1703/recipes-fsl/images/fsl-image-kernelitb.bbappend


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,430件の閲覧回数
mounikareddy22
Contributor I

Hi,

Thank you for the reply..!

I have few more doubts:

1. Were I can download the fsl-image-kernelitb.bbappend ?

2. If I download and add the fsl-image-kernelitb.bbappend file to recipe folder will it work straight away or I need to do any changes?

Could you please suggest me the procedure?

Thanks & Regards,

Mounika Anugula

Design Engineer

Mobile : (+91) 9916711639

Website : <http://www.coreel.com> www.coreel.com

Ph: (+91)80-41970400

Fax: (+91)80-30723638

CoreEL Technologies,

#21, 7th Main, 1st Block , Koramangala,

Bangalore 560034

<https://www.facebook.com/CoreELTechnologies> Description: Description: Image result for facebook icon in orange <https://www.linkedin.com/company/coreel-technologies?trk=company_logo> Description: Description: Image result for facebook icon in orange

Description: COREEL~1 - Copy.JPG

0 件の賞賛
返信