frdm-ls1012a update u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

frdm-ls1012a update u-boot

1,405 Views
mukunkong
Contributor I

I exec command in u-boot `sf write 0x96000000 0x20000 $uboot-filesize` in my new board(frdm-ls1012a-pa),nothing log with serial console,u-boot.bin file is build through yocto project,can you tell me how to update u-boot for frdm-ls1012a,thanks 

0 Kudos
Reply
1 Reply

1,266 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello 穆 昆空,

The Start Address of u-boot should be at 0x40100000, offset 0x100000 on QSPI flash.

 

=>tftp 0x80000000 <u-boot_file_name>.bin

=>sf probe 0:0

=>sf erase 0x100000 +$filesize

=>sf write 0x80000000 0x100000 $filesize

=> reset


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply