flash routines

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flash routines

2,627件の閲覧回数
ramadasr
Contributor I

Hi,

I am working on BSP for P2041 processor, where can I find eLBC configuration routines( for all the machines)  and also low level write erase routines for NOR and NAND flash? Thanks,

Ramadas

タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,432件の閲覧回数
marius_grigoras
NXP Employee
NXP Employee

Hi Ramadas,

Check this out -> include\configs\P2041RDB.h from u-boot source files.

Regards,

Marius

0 件の賞賛
返信

2,432件の閲覧回数
sinanakman
Senior Contributor III

Hi Ramadas, for NOR flash please refer to the CFI interface and erase command in your flash data sheet. For NAND flash you will find this information in P2041 Reference Manual in the section that describes the flash controller. Hope this helps

Sinan Akman

0 件の賞賛
返信

2,432件の閲覧回数
Wei
Contributor I

Have you checked the u-boot source code?

0 件の賞賛
返信