enable USB test pattern

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

enable USB test pattern

6,778件の閲覧回数
pipapo
Contributor I

How to enable USB test pattern on LS1046A?

Found register USBxDCTL[TSTCTL].

Write to TSTCTL bits have no effect

0 件の賞賛
返信
7 返答(返信)

5,817件の閲覧回数
christianwächte
Contributor I

Our FAE provided a solution for this problem. To start the USB 2.0 test pattern generation on the LS1046A via u-boot, you have to enter these commands:

usb start
mw.l 3100420 0
mw.l 3100430 0
mw.l 3100020 0
mw.l 3100424 50000000
mw.l 3100020 1

These are the commands for USB 3.0 controller 3. Change the offset to the following for accessing the other USB ports

USB3.0 controller 1 -->  2F0_0000 - 2FF_FFFF

USB3.0 controller 2 --> 300_0000 - 30F_FFFF

USB3.0 controller 3 --> 310_0000-31F_FFFF

The state of the USB_ID Pin seem to have no effect on the test pattern output

0 件の賞賛
返信

5,817件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at attached file. Find the dwc3_gadget_set_test_mode() procedure in these files. It is part uf u-boot USB driver for the LS1046a USB from LSDK 1712. The same procedure is used in kernel USB driver for setting USB TEST MODES.

Use this procedure for TEST mode setting.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,817件の閲覧回数
christianwächte
Contributor I

I saw that there are these functions in u-boot but had no success. I tried various testmodes on the correct USB port and device. Is there any application note or best practise on this topic you can provide?

Just to make sure, we are talking about the same thing: I'm trying to output the USB test pattern of the USB 2.0 part. The test pattern for USB 3.0 have been output automatically and are working find.

Best regards,

Christian Wächter

0 件の賞賛
返信

5,817件の閲覧回数
christianwächte
Contributor I

I have a new information saying that I have to write to the PORTPMSC register at offset 0x424, because my device is is USB host mode (it's a industrial PC). Register DCTL is for USB device mode.

Unfortunatelly I do not find any information about the PORTPMSC register, e.g. which fields are included and which bits have to be set...

0 件の賞賛
返信

5,817件の閲覧回数
christianwächte
Contributor I

Is there anyone who knows a way to enable the output of the USB test pattern via the DCTL register (Reference Manual, page 2534), that contains the TSTCTL field?

I haven't had any success with the files from the SDK

0 件の賞賛
返信

5,817件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at attached files. These files are used for setting test modes on the LS1043ARDB board. These files are part SDK 2.0 USB driver.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,817件の閲覧回数
christianwächte
Contributor I

Hello Pavel,

thank you for your reply. I will try your suggestion in the next days.

Is there a possibility to write the according values directly into the registers without linux, e.g. while in u-boot? I tried this but haven't had any success.

Best regards,

Christian Wächter

0 件の賞賛
返信