difference in ls1043A-RGW ls1043A-RGW-B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

difference in ls1043A-RGW ls1043A-RGW-B

1,220件の閲覧回数
klh
Contributor I

Hi, may I know what is the difference between ls1043 cpu rev A (1.0) vs rev B (1.1) as in ls1043A RGW? thx

0 件の賞賛
返信
1 返信

1,093件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the LS1043a AN5012 Design Check List Rev. 3 about different SVR for these revisions:

https://www.nxp.com/webapp/Download?colCode=AN5012&Parent_nodeId=1412692250778715498030&Parent_pageT...

 

The LS1043A rev B (1.1) supports the following:

host OS with 64 KB page size requirement

 

Each PCI Express message signaled interrupts (MSI) supports four serial peripheral interface (SPI) interrupts

 

CoreLink generic interrupt controller (GIC-400) memory map supports both 4 KB and 64 KB granularity through a programmable bit in SCFG map


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信