can't find firmware file in yocto build folder

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can't find firmware file in yocto build folder

Jump to solution
7,212 Views
rans
Senior Contributor I

Hello,

 

I hope someone can help with the following.

I've build yocto image for ls1046ardb (I've bitbaked for both main and tiny images)

Yet, I don't find any firmware file (firmware_ls1046ardb_sdboot.img) , and also can't find any kernel file (
( boot_ls1043ardb_lts_6.1.tgz ),

Thanks,

rans

0 Kudos
Reply
1 Solution
7,127 Views
rans
Senior Contributor I

the user/password is: user/user

I am not sure why it is not written in documentation....

I also suggest to add the command " bitbake generate-boottgz" to table 7 (3.5.4), it may save others who struggled on the same stuff  

 

View solution in original post

0 Kudos
Reply
7 Replies
7,137 Views
rans
Senior Contributor I

I found the problem, I had to run

bitbake generate-boottgz

now I can see the boot file, thanks,

0 Kudos
Reply
7,174 Views
rans
Senior Contributor I

@LFGP 

Sure, the steps are as described in  Rev. L6.1.36_2.1.0 — 9 November 2023 , chapter 3.7.7 (LS1046ARDB) and chapter 3.5.4 - bitbake commands  i.e.

DISTRO=fsl-qoriq-distro MACHINE=ls1046ardb source distro-setup-env
$ bitbake ls-image-main

and

bitbake qoriq-composite-firmware

and then I would like prepare SD as mentioned in step 4

Writing image to SD card:

 

$ flex-installer -b tmp/deploy/image/<board> bootp_xxx.tgz -r tmp/deploy/image/<board>/ls-image-main-xxx.tar.gz -f tmp/ deploy/image/<board>/firmware_sdboot_secure.img -d /dev/ sdx

 

But though I have the firmware<> file and rootfs file ls-image-main<>.tar.gz, I still can't find any boot<>_file (not file starts with boot prefix)

  • Is it some other file maybe ? (see the original post with file list)
  • Is the tiny build should be used only for minimal boot and for programming other storage device ? If this is the case it means that flash qspi can't be used for booting customized linux, Right ?

Thanks!

rans

 

0 Kudos
Reply
7,154 Views
LFGP
NXP TechSupport
NXP TechSupport

@rans 

regarding your questions:

  • Is it some other file maybe ? answ: no, the mentioned are the rights.

 

  • Is the tiny build should be used only for minimal boot and for programming other storage device ? answ: Yes, it is intended for that.
  • If this is the case it means that flash qspi can't be used for booting customized linux, Right ? answ: right.

Please share the  output logs in order to analyze them and try to detect  some missing, due from my side the images was generated as expected. 

0 Kudos
Reply
7,191 Views
LFGP
NXP TechSupport
NXP TechSupport

please share with me the steps you are following  to try to generate the images, and also please share the log when you do bitbake.
I need to check if something was missing or if there something wrong.

7,122 Views
rans
Senior Contributor I

Hi @LFGP 

After installing the build (as-is from sources) yocto and deploying it in SD card, I insert card, and starts boot, but then in login, I can't pass the login...

I tried login: root, but it then asks for password (?)

ls1046ardb login: root
Password:

I tried to enter in password: just enter/root/... but nothing passes.

see complete boot log from sd

Any idea ?

rans

0 Kudos
Reply
7,128 Views
rans
Senior Contributor I

the user/password is: user/user

I am not sure why it is not written in documentation....

I also suggest to add the command " bitbake generate-boottgz" to table 7 (3.5.4), it may save others who struggled on the same stuff  

 

0 Kudos
Reply
7,128 Views
rans
Senior Contributor I

Hi @LFGP 

Thanks a lot for the assistance

please see attached log,

0 Kudos
Reply