I have downloaded BSP for a Power PC platform successfully modified according to needs of the custom target board and the application is running. Now I would like to create the ISO for the modified BSP so as to distribute to the end users. What are the commands to do so. Running this command should not wipe out my existing modified settings.
Hello vishnu prasad,
Please refer to the attached script, which we are using to generate Yocto release ISO.
Usage:
./giso.sh -d yocto_dir -p iso_prefix -c cache_compress_type
-d the full path of yocto folder
-p prefix of generated ISO name
-c cache packages compress type, value can be xz, bzip2 or gzip.
default compress type is xz.
Eg: $ ./giso.sh -p QorIQ-DPAA-SDK -d <path-of-yocto>
Thanks,
Yiping