boot method of ARDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

boot method of ARDB

跳至解决方案
2,369 次查看
junfeng_zhang
Contributor I

Dear NXP(ARDB) expert:

Thank you very much. 

BR/Junfeng

0 项奖励
回复
1 解答
2,011 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the following Community question:

https://community.nxp.com/message/1079924 

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,011 次查看
ufedor
NXP Employee
NXP Employee
0 项奖励
回复
2,011 次查看
junfeng_zhang
Contributor I

Thank you Ufedor:)

BR/Junfeng

0 项奖励
回复
2,011 次查看
ufedor
NXP Employee
NXP Employee

There is no pre-built SD boot image for the LS2088ARDB.

Please use a debugger and restore NOR or QSPI firmware image available at:

LSDK Open Source 

LSDK IMAGES

0 项奖励
回复
2,012 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the following Community question:

https://community.nxp.com/message/1079924 

0 项奖励
回复
2,011 次查看
ufedor
NXP Employee
NXP Employee

On the LS2085ARDB/LS2088ARDB revisions D – F, switch SW9 bits 3:5 control which bank the SoC loads from when it powers up.

When SW9[3:5] = OFF-OFF-OFF - NOR Flash Bank 0 is selected. With this settings the NOR Flash bank 0 is started from address 0x580000000.

0 项奖励
回复