Where can I find the source code fo the NXP PCI Endpoint device driver ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I find the source code fo the NXP PCI Endpoint device driver ?

2,419件の閲覧回数
peterjdonovan
Contributor I

Need to create a PCIe  endpoint on a p2040.  NXP documention refers to "VFIO support for NXP Endpoint devices" but I cannot find the code for the driver anywhere.

ラベル(1)
タグ(1)
2 返答(返信)

2,105件の閲覧回数
peterjdonovan
Contributor I

Thank you Pavel. I will give it a shot.

-Peter

0 件の賞賛
返信

2,105件の閲覧回数
Pavel
NXP Employee
NXP Employee

See the Chapter 7.11 of SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

Draw attention on the Section 7.11.6

Have a great day,
Pavel Chubakov

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------