Watchdog does not work on LS1020A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Watchdog does not work on LS1020A

2,186 次查看
nagireddychitta
Contributor III

Hi All,

I am in need of enabling watchdog to reset/reboot the system.

I have tried setting up watchdog1 counter for 8 seconds and then enable the watchdog. My observation is that, watchdog resets the system(i believe it is 0.5 sec as per reference manual) as soon as i enable the watchdog and it won't really wait for counter to timeout.

I have then i tried the same on watchdog 2 but the result is that it never resets the system.

Pls see the below Uboot log:

//////////////////////////////////////////////////////////////////////////////////////////////////////////////////

U-Boot 2015.01+SDKv1.9+geb3d4fc (Aug 03 2016 - 04:01:00)

CPU:   Freescale LayerScape LS1020, Version: 2.0, (0x87001020)

Clock Configuration:

       CPU0(ARMV7):1000 MHz,

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

       00000000: 0608000a 00000000 00000000 00000000

       00000010: 00000000 00407908 e0025a00 21046000

       00000020: 00000000 00000000 00000000 00018000

       00000030: 00080000 881b7340 00000000 00000000

Board: NEXTFLASH

I2C:   ready

DRAM:  2 GiB

Using SERDES1 Protocol: 0 (0x0)

Flash: 128 MiB

PCIe1: Root Complex x4 gen2, regs @ 0x3400000

PCIe1: Bus 00 - 01

PCIe2: disabled

In:    serial

Out:   serial

Err:   serial

SCSI:  Net:   eTSEC3 [PRIME]

Hit any key to stop autoboot:  0

=> mm.b 0x2ad0000   --> First Watchdog timer

02ad0000: 00 ? 10      --> Setting timeout for 8 seconds

02ad0001: 30 ? 04      --> Enabling the Watchdog

--> System gets reset immediately.

U-Boot 2015.01+SDKv1.9+geb3d4fc (Aug 03 2016 - 04:01:00)

CPU:   Freescale LayerScape LS1020, Version: 2.0, (0x87001020)

Clock Configuration:

       CPU0(ARMV7):1000 MHz,

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

       00000000: 0608000a 00000000 00000000 00000000

       00000010: 00000000 00407908 e0025a00 21046000

       00000020: 00000000 00000000 00000000 00018000

       00000030: 00080000 881b7340 00000000 00000000

Board: NEXTFLASH

I2C:   ready

DRAM:  2 GiB

Using SERDES1 Protocol: 0 (0x0)

Flash: 128 MiB

PCIe1: Root Complex x4 gen2, regs @ 0x3400000

     01:00.0    - 1235:7024 - Memory controller

PCIe1: Bus 00 - 01

PCIe2: disabled

In:    serial

Out:   serial

Err:   serial

SCSI:  Net:   eTSEC3 [PRIME]

Hit any key to stop autoboot:  0

=> mm.b 0x2ae0000 --> Second Watchdog timer

02ae0000: 00 ? 10

02ae0001: 30 ? 04

02ae0002: 00 ? --> No system reset at all

/////////////////////////////////////////////////////////////////////////////////////////////////////

Is there any issue with watchdog timers in LS1020A SoC or am i missing any sequence ? Kindly help.

Regards,

Nagi

0 项奖励
回复
2 回复数

1,901 次查看
ufedor
NXP Employee
NXP Employee

02ad0000: 00 ? 10      --> Setting timeout for 8 seconds

02ad0001: 30 ? 04      --> Enabling the Watchdog

Is there any difference when the WDOG1_WCR is accessed as 16-bit register?

0 项奖励
回复

1,901 次查看
nagireddychitta
Contributor III

Hi ufedor,

Pls see below:

Byte operations can be performed on these registers as per the reference manual of LS1021/LS1020.

Hit any key to stop autoboot:  0

=> mm.b 0x2ad0000   --> First Watchdog timer

02ad0000: 00 ? 10      --> Setting timeout for 8 seconds

02ad0001: 30 ? 04      --> Enabling the Watchdog

--> System gets reset immediately.

pastedImage_0.png

I have also tried 16bit access but the result is same.

Best Regards,

Nagi

0 项奖励
回复