Use space GPIO sysfs interface not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use space GPIO sysfs interface not working

1,689件の閲覧回数
michaelchen_nsb
Contributor II

Dear NXP yipingwang ufedor ,

Currently in our project, which is base on LS1048A, GPIO sysfs interface cannot work probably, and we need your help.

Here is the detail.

We can manually control the GPIO through devmem2 tool. For example, PHY_RESET is GPIO3_23 and SFP_LED is GPIO3_27,so we can use devmem2 to control both GPIOs

devmem2 0x2320000 w 0x00000110

devmem2 0x2320008 w 0x00000110

devmem2 0x2320018 w 0x00000110

But, when wen use GPIO sysfs interface, it's didn't work, and when we operate SFP_LED, it has impact on PHY_RESET, and we can see lots of abnormal print as followed.

root@ls1088ardb:~# echo 443 > /sys/class/gpio/export

root@ls1088ardb:~# echo out > /sys/class/gpio/gpio443/direction

root@ls1088ardb:~# [ 161.276474] mdio_bus 8b96000: Error while reading PHY1 reg at 1.1 [ 161.282669] mdio_bus 8b96000: Error while reading PHY1 reg at 1.1 [ 161.288864] mdio_bus 8b96000: Error while reading PHY1 reg at 10.10 [ 161.295219] mdio_bus 8b96000: Error while reading PHY1 reg at 9.9 [ 161.301406] mdio_bus 8b96000: Error while reading PHY1 reg at 5.5 [ 161.307587] mdio_bus 8b96000: Error while reading PHY1 reg at 4.4 [ 161.313772] mdio_bus 8b96000: Error while reading PHY1 reg at 1.1

Looking forward to hear from you soon.

Best regards

Chen Feng

0 件の賞賛
返信
1 返信

1,564件の閲覧回数
Pavel
NXP Employee
NXP Employee

There is technical case from you about this problem. See information in this technical case.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信