Unable to ping to u-boot in T2080RDB from Linux host PC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to ping to u-boot in T2080RDB from Linux host PC

Jump to solution
2,356 Views
singhawadhesh
Contributor I

Hi Team,

I have enabled the 1G RGMII (RTL8211E) ethernet ports (Port FM1@DTSEC3 in U-boot and port fm1-mac3 in linux) on the t2080 reference board, assigned IP address using dhcp. However, I am unable to ping to the t2080 board u-boot from the linux PC.

From U-boot if I try this connection (ping 10.60.101.107) I get a response. But since linux I configure the network but I do not get the answer.

In linux I follow the following steps to configure the network:

1) vi /etc/network/interfaces

2) I add the following lines in the interface file:

      auto fm1-mac3

      iface fm1-mac3 inet static

      address 10.60.101.109

      net mask 255.255.255.0

3) From the console I execute:

      ifup  -a fm1-mac3

4) Then I try ‘ping 10.60.101.109’ but I can’t.

From U-boot if I do 'ping 10.60.101.107', I get the following response:

      Using FM1@DTSEC3 device

      host 10.60.101.107 is alive

Note: I am not sure if I will get response when I will ping to t2080 u-boot from Linux host system.

 

Thanks and Regards,

Awadhesh Singh

 

 

0 Kudos
Reply
1 Solution
2,351 Views
yipingwang
NXP TechSupport
NXP TechSupport

U-Boot doesn't respond back to ARP(ping) requests.

So you cannot get responding from u-boot, when ping T2080RDB from Linux host PC.

View solution in original post

0 Kudos
Reply
1 Reply
2,352 Views
yipingwang
NXP TechSupport
NXP TechSupport

U-Boot doesn't respond back to ARP(ping) requests.

So you cannot get responding from u-boot, when ping T2080RDB from Linux host PC.

0 Kudos
Reply