U-boot DDR Initialization with and Without Codewarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-boot DDR Initialization with and Without Codewarrior

1,678 Views
tmorrison
Contributor III

I am booting out SD Card, and I am failing to boot when I hit reset and allow it run natively.

I have tracked it down to the DDR Init Done bit (*SDRAM_CFG2_ADDR & 0x10) never resets 

(indicating completion. 

BUT when I debug using CodeWarrior - it works like a charm. 

Is there some guidance on a thing like this?

0 Kudos
Reply
1 Reply

1,606 Views
yipingwang
NXP TechSupport
NXP TechSupport

You could use attach method to debug u-boot, please refer to the section "2. Debug u-boot with CodeWarrior for ARMv8" in Use CodeWarrior for ARMv8 to Debug U-boot and Linux Kernel and Bring up Bare Boards to attach to the running u-boot to do debugging.

0 Kudos
Reply