Two CST versions calculate different hashes for same key

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Two CST versions calculate different hashes for same key

1,791件の閲覧回数
nenadradulovic
Contributor I

Hello,

I have been using 17.06 LayerScape SDK successfully on LS1021A-TWR board and enabled Secure Boot with Confidentiality. The CPU was burned with OTPMK and SRK and everything works as expected.

Now I need to test the 17.09 SDK. The first thing I noticed during building is that CST utilities now print different hashes although the same keys were used (srk.pub and srk.pri), copied from previous project version. The board doesn't boot now, perhaps due to wrong key values being used.

What has changed? I've copied the two files (mentioned above) to CST build directory, am I missing something?

The commit from 17.09 (non-working) is 1afb40c13097fc9e8a641aa5d0420498fea01c65

The commit from 17.06 (working) is 6424157985568df3f42a46e24222e38671455ddb


					
				
			
			
				
			
			
				
			
			
			
			
			
			
		
タグ(5)
0 件の賞賛
返信
2 返答(返信)

1,686件の閲覧回数
nenadradulovic
Contributor I

Hello, I did overcome this by disregarding the last commit in cst apps:

flex-builder -i repo-fetch

flex-builder -i repo-tag

cd packages/apps/cst

git checkout HEAD~1

cd -

continue with usual command sequence...

Best regards,

Nenad

0 件の賞賛
返信

1,686件の閲覧回数
nenadradulovic
Contributor I

Hello, I've found that the last commit in LSDK-17.09 branch has changed the behavior of CST. The commit is:

1afb40c13097fc9e8a641aa5d0420498fea01c65

Make SRK table default option

Since in ls1088ardb and 2088ardb, by default srk table is assumed, even if single key is present, making it common for all platforms

case FIELD_KEY_SELECT:
474474 if (file_field.count == 1) {
475475 gd.srk_sel = STR_TO_UL(file_field.value[0], 16);
476-gd.srk_flag = 1;
477476 } else {
478477 gd.srk_sel = 1;
479478 }
479+gd.srk_flag = 1;
480480 
481481 break;

Why is this relevant to how the hash is calculated?

0 件の賞賛
返信