T4240 IFC CONTROLLER

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T4240 IFC CONTROLLER

1,467件の閲覧回数
venkatesansathy
Contributor I

Hi,

I want interface 4 NOR flashes with IFC of T4240  without FPGA. Is it possible with latch and buffer only ,please clarify.

Thanks&Regards

Venkatesan sathyamoorthy

0 件の賞賛
返信
1 返信

1,254件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Using FPGA is not mandatory to connect NOR Flash to IFC controller, you can do that only with latch.

Please look FIgure 12-6 in T4240 Reference Manual for NOR flash connection part.

If you want to connect 4 NOR flashes, please use remaining chip select lines CE[1:3] to drive NOR flash CE_B inputs, all other signals should be connected in parallel.

Voltage buffer is necessary, if your NOR flash I/O voltage is not the same as T4240 IFC controller output voltage.

Please also keep in mind total capacitance of all pins connected to AD bus and their effect to IFC timings.

When you attach large capacitance to output driver, its output timings are affected by RC-time, where R is effective output resistance of I/O driver, and C is capacitance of load connected. Placing extra load capacitance causes extra delays at output signals, and may affect IFC bus timings and finally affect bus throughput.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信