T4080 Bring up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4080 Bring up

3,304 Views
muralikothandap
Contributor I

When I try to program the NOR Flash using the U-Boot binaries, I get Sector Protection Error. Can you please advice what is wrong.

Original Attachment has been moved to: T4160_FlashProg_log.txt.zip

0 Kudos
Reply
1 Reply

3,199 Views
Pavel
NXP Employee
NXP Employee

Test your configuration on the T4080RDB board.

Check Flash programmer setting for your Flash.

 

Look at the AppNote-FlashProgrammer-PowerArchitecture.pdf file, This file is available in CodeWarrior folder using the following path:

C:\Freescale\CW_PA_v10.5.1\PA\PA_Tools\FlashToolKit\Documentation

 

This file also is available in the attachment.

 

Use this file to add new Flash in CodeWarrior Flash Programmer.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply