T2080RDB u-boot arguments gone wrong

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080RDB u-boot arguments gone wrong

2,010 次查看
vojislavmokric
Contributor I

Hi All,

I wanted to change initial u boot arguments/variables to enable Ethernet connection, but once I change them and save them, my board doesn't boot up any more. Here is the log:

I'm kinda new in these things, so if some of you guys with more experience could have a look and give me some clues.

I have changed:

ethprime

netmask

gatewayip

ipaddr

Thanks,

Vojislav

U-Boot 2014.07QorIQ-SDK-V1.7+g659b6a2 (Jan 02 2015 - 11:30:53)                 

                                                                               

CPU0:  T2080E, Version: 1.1, (0x85380011)                                      

Core:  e6500, Version: 2.0, (0x80400120)                                       

Clock Configuration:                                                           

       CPU0:1799.820 MHz, CPU1:1799.820 MHz, CPU2:1799.820 MHz, CPU3:1799.820 M

       CCB:666.600 MHz,                                                        

       DDR:799.980 MHz (1599.960 MT/s data rate) (Asynchronous), IFC:166.650 MHz

       FMAN1: 699.930 MHz                                                      

       QMAN:  333.300 MHz                                                      

       PME:   666.600 MHz                                                      

L1:    D-cache 32 KiB enabled                                                  

       I-cache 32 KiB enabled                                                  

Reset Configuration Word (RCW):                                                

       00000000: 1406001b 15000000 00000000 00000000                           

       00000010: 66150002 00000000 ec027000 c1000000                           

       00000020: 00800000 00000000 00000000 000307fc                           

       00000030: 00000000 00000000 00000000 00000004                           

Board: T2080RDB, Board rev: 0x01 CPLD ver: 0x03, boot from NOR vBank0          

SERDES Reference Clocks:                                                       

SD1_CLK1=156.25MHZ, SD1_CLK2=100.00MHZ                                         

SD2_CLK1=100.00MHZ, SD2_CLK2=100.00MHZ                                         

I2C:   ready                                                                   

SPI:   ready                                                                   

DRAM:  Initializing....using SPD                                               

Detected UDIMM 18KSF51272HZ-1G6K2                                              

4 GiB (DDR3, 64-bit, CL=11, ECC on)                                            

       DDR Chip-Select Interleaving Mode: CS0+CS1                              

Flash: 128 MiB                                                                 

L2:    2 MiB enabled                                                           

Corenet Platform Cache: 512 KiB enabled                                        

Using SERDES1 Protocol: 102 (0x66)                                             

Using SERDES2 Protocol: 21 (0x15)                                              

NAND:  512 MiB                                                                 

MMC:   FSL_SDHC: 0                                                             

EEPROM: NXID v1                                                                

PCIe1: Endpoint, no link, regs @ 0xfe240000                                    

PCIe1: Bus 00 - 00                                                             

PCIe2: Root Complex, x2 gen2, regs @ 0xfe250000                                

  02:00.0     - 1957:0808 - Processor                                          

PCIe2: Bus 01 - 02                                                             

PCIe3: disabled                                                                

PCIe4: Root Complex, no link, regs @ 0xfe270000                                

PCIe4: Bus 03 - 03                                                             

In:    serial                                                                  

Out:   serial                                                                  

Err:   serial                                                                  

Net:   Fman1: Uploading microcode version 106.4.14                             

PHY reset timed out                                                            

PHY reset timed out                                                            

FM1@DTSEC3, FM1@DTSEC4, FM1@TGEC1, FM1@TGEC2, FM1@TGEC3, FM1@TGEC4             

Hit any key to stop autoboot:  0                                               

WARNING: adjusting available memory to 30000000                                

Wrong Image Format for bootm command                                           

ERROR: can't get kernel image!             

                                  

=> printenv                                                                    

baudrate=115200                                                                

bdev=sda3                                                                      

bootargs=root=/dev/ram rw console=ttyS0,115200                                 

bootcmd=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootr

bootdelay=10                                                                   

bootfile=uImage                                                                

consoledev=ttyS0                                                               

eth1addr=00:04:9F:03:49:B3                                                     

eth2addr=00:04:9F:03:49:AE                                                     

eth3addr=00:04:9F:03:49:AF                                                     

eth4addr=00:04:9F:03:49:B0                                                     

eth5addr=00:04:9F:03:49:B1                                                     

ethact=FM1@DTSEC3                                                              

ethaddr=00:04:9F:03:49:B2                                                      

ethprime=fm1-mac3                                                              

fdtaddr=0x00c00000                                                             

fdtfile=t2080rdb/t2080rdb.dtb                                                  

fman_ucode=eff00000                                                            

gatewayip=10.10.0.1                                                            

hwconfig=fsl_ddr:ctlr_intlv=cacheline,bank_intlv=auto;usb1:dr_mode=host,phy_typi

ipaddr=10.10.1.110                                                             

loadaddr=0x1000000                                                             

netdev=eth0                                                                    

netmask=255.255.254.0                                                          

nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddrr

ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootr

ramdiskaddr=0x02000000                                                         

ramdiskfile=t2080rdb/ramdisk.uboot                                             

rootpath=/opt/nfsroot                                                          

stderr=serial                                                                  

stdin=serial                                                                   

stdout=serial                                                                  

tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize && erae

uboot="u-boot.bin"                                                             

ubootaddr=0xeff40000                                                           

                                                                               

Environment size: 1669/8188 bytes

标记 (2)
0 项奖励
回复
3 回复数

1,652 次查看
karunakaranradh
Contributor IV

Hi Vojislav,

I assumed you are try to boot Linux with ramdisk filesystem based on the environmental variable "root=/dev/ram"

If you wants to boot Linux with ramdisk filesystem change the bootarg and bootcmd as follows

=> setenv bootargs "'root=/dev/ram rw console=ttyS0,115200 ramdisk_size=<size of ramdisk>'"

=> setenv bootcmd "'bootm <starting address of Kernel> <starting address of ramdisk> <starting address of device tree>'"

Example:

Assume kernel image is in 0xE8020000,  ramdisk rootfs is in 0xED300000 and Hardware device tree is in 0xE8800000 location then set the following environmental variable.

=> setenv bootcmd "'bootm 0xE8020000 0xED300000 0xE8800000'"

Regards

Karuanakaran R

0 项奖励
回复

1,652 次查看
bpe
NXP Employee
NXP Employee

u-Boot says your kernel image is broken, but it is not possible

to tell what exactly is wrong because your terminal truncated long lines

of the output of printenv command. Please configure your terminal to

wrap long lines, execute printenv and re-submit the output.

0 项奖励
回复

1,652 次查看
bpe
NXP Employee
NXP Employee

You are asking in a wrong community. T2080 is not an i.MX processor. Please move your post to the QorIQ community.

0 项奖励
回复