T2080 Refernce Design RTC INT Pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 Refernce Design RTC INT Pin

1,775件の閲覧回数
hemanttiwari199
Contributor III

In T2080 Refernce board schematic, why INT PIN OF DS1339U-33+ RTC is Pulled up by 1.8V?

As the IC operating Voltage is 3.3V it should be pulled up using 3.3V and then using level translator it should connect to 1.8V of T2080 pin.

Can you explain the logic behind this connection?


Regards

Hemant 

タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,737件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the DS1339U-33 Data Sheet where it is written:

"The SQW/INT pin is an open-drain output and requires an external pullup resistor."

0 件の賞賛
返信

1,737件の閲覧回数
hemanttiwari199
Contributor III

yes, it is require pull up resistor, but my concern is related to voltage.

DS1339U works on 3.3V and SQW/INT pin is connected to t2080 IRQ pin having pull up resistor having 1.8V.

how the connection are going to work because of the pullup voltage difference?

0 件の賞賛
返信

1,737件の閲覧回数
ufedor
NXP Employee
NXP Employee

To understand how open collector/drain works it is needed to read, for example:

Open collector - Wikipedia 

0 件の賞賛
返信

1,737件の閲覧回数
hemanttiwari199
Contributor III

Can you please explain me using some reference ?

0 件の賞賛
返信