T2080 Ref Clock Requirement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 Ref Clock Requirement

1,407 Views
tomr2020
Contributor I

We are adding 10G XFI to a T2080 board. The reference clock requirements seems to tough to meet. The Total jitter is spec'd at 11ps. Is there a chance that this is 11ps RMS instead of total Jitter?  Anyone have an oscillator that will do this if its not RMS? Table 61 of the data sheet. Thanks Tom

Tags (2)
0 Kudos
Reply
1 Reply

1,261 Views
alexander_yakov
NXP Employee
NXP Employee

The total jitter = total deterministic jitter + 14.069 * square root of sum of random jitter squared assuming BER 10E-12. thus answer to your question is yes take the RMS of random jitter at integration range then multiply it by 14.069 then add any deterministic jitter to the sum which should be under 11ps per our spec. In our RM we used a part similar to:

https://www.idt.com/document/dst/8t49n222i-datasheet


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply