T2080 Processor integration with DDR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 Processor integration with DDR

1,242 Views
Vanam_Balaraju
Contributor I

Hi Team,

We are using T2080 sereis Processor (Part # T2080NXE8M) in one of our project

1. as per requirement we need to integrate Processor T2080 with 8GB DDR3

2. Due to non availability of 8GB DDR3, we are using 4# 2GB DDR3

3. As per T2080 spec. 64-bit DDR3 memory controller with ECC support is available  then we wants to connect 4# 16-bit 2GB DDRs with T2080 Processor

4. Hence requesting you to please let us know these kind of hardware architecture is allowed and possible?

Thank you

Regards

Vanam Bala Raju

 

 

 

0 Kudos
Reply
1 Reply

1,202 Views
June_Lu
NXP TechSupport
NXP TechSupport

For the general support of DDR SDRAM device configurations, you could refer to QorIQ T2080 Reference Manual, page 510, Table 12-8. Supported DDR3 SDRAM Device Configurations

For the architecture is not included, should provide the specific configuration and datasheet to confirm.

Thanks

0 Kudos
Reply