T2080 Processor integration with DDR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 Processor integration with DDR

1,271件の閲覧回数
Vanam_Balaraju
Contributor I

Hi Team,

We are using T2080 sereis Processor (Part # T2080NXE8M) in one of our project

1. as per requirement we need to integrate Processor T2080 with 8GB DDR3

2. Due to non availability of 8GB DDR3, we are using 4# 2GB DDR3

3. As per T2080 spec. 64-bit DDR3 memory controller with ECC support is available  then we wants to connect 4# 16-bit 2GB DDRs with T2080 Processor

4. Hence requesting you to please let us know these kind of hardware architecture is allowed and possible?

Thank you

Regards

Vanam Bala Raju

 

 

 

0 件の賞賛
返信
1 返信

1,231件の閲覧回数
June_Lu
NXP TechSupport
NXP TechSupport

For the general support of DDR SDRAM device configurations, you could refer to QorIQ T2080 Reference Manual, page 510, Table 12-8. Supported DDR3 SDRAM Device Configurations

For the architecture is not included, should provide the specific configuration and datasheet to confirm.

Thanks

0 件の賞賛
返信