T2080 IBIS model problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 IBIS model problem

1,339件の閲覧回数
anandram
Contributor I

Hi,

We are using T2080 in our custom board,I'm try to do post SI simulation for T2080 serdes interfaces in Hyperlynx tool.But I'm not able to carry simulation for serdes TX lines of T2080,where simulation tool is crashing whenever i assign TX model.Please help.

0 件の賞賛
返信
1 返信

1,209件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Hello,

T2080 IBIS model is not public. We can not debug the problem in public, to debug the problem please open a case to online technical support. When opening a case, please do not forget to specify which IBIS model you are using, exact file name will be enough.

To enter a case to online technical support please perform the following:

1. Open www.nxp.com

2. Click on "Account" or your name in upper right corner and select "My account", enter your NXP site login/password if necessary.

3. Select "View all Support Methods" in Support section.

4. Click "Go to Tickets" in "Support Requests" section

5. The system should redirect you to this page https://nxpcommunity.force.com/community/CommunityContextPage 

6. At this page please create a new folder for support cases by clicking "Add a Folder". Typically - one folder per project.

7. When asked, enter project details - design stage, projected annual volume, end application type and application name.

8. When folder is created, please click "Add a new case" button to create support case.

Have a great day,
Alexander
TIC

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 件の賞賛
返信