T2080:Audio Interfacing support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080:Audio Interfacing support

2,063 Views
anandram
Contributor I

Hi we have used T2080 processor in one of our design,now there is a requirement from the customer on Audio interfacing.

I would like to know does T2080 support audio controller? If not,please suggest is there any way to implement audio interfacing on this chip.

0 Kudos
Reply
3 Replies

1,988 Views
alexander_yakov
NXP Employee
NXP Employee

No, T2080 processor does not have audio controller. I can only suggest using external chip connected to any of available communication interfaces. We do not offer a ready-to-use solution to this case, sorry.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,988 Views
anandram
Contributor I

Hi Alexandar,

Thaks for the reply,

Can you please suggest me any external Audio dac chip that can be compatible to use with T2080.

0 Kudos
Reply

1,988 Views
alexander_yakov
NXP Employee
NXP Employee

We do not offer a ready-to-use solution to this case, sorry.

0 Kudos
Reply