T1042 - PCIe link Loopback Test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042 - PCIe link Loopback Test

1,682 Views
skittikh
Contributor I

Using T1042, would like to test the PCIe links by loopback the TX to RX.  Is there any internal registers of T1042 that we can use to verify whether the links are working?

0 Kudos
Reply
1 Reply

1,501 Views
ufedor
NXP Employee
NXP Employee

Digital loopback can be enabled by setting corresponding SerDes_LNnTCSR3[LPBK_EN]=0b01.

External loopback can be tested in application mode using external loopback add-in card or by connecting TX to RX signals through AC coupling capacitors at the backplane.

0 Kudos
Reply