T1042 - PCIe link Loopback Test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1042 - PCIe link Loopback Test

1,681件の閲覧回数
skittikh
Contributor I

Using T1042, would like to test the PCIe links by loopback the TX to RX.  Is there any internal registers of T1042 that we can use to verify whether the links are working?

0 件の賞賛
返信
1 返信

1,500件の閲覧回数
ufedor
NXP Employee
NXP Employee

Digital loopback can be enabled by setting corresponding SerDes_LNnTCSR3[LPBK_EN]=0b01.

External loopback can be tested in application mode using external loopback add-in card or by connecting TX to RX signals through AC coupling capacitors at the backplane.

0 件の賞賛
返信