T1040 flush cache

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1040 flush cache

5,899 Views
hv
Contributor II

for the T1040RDB, if I want to flush cache, do I need to flush L1 and L2 backside cache separately? 

0 Kudos
Reply
6 Replies

5,680 Views
LPP
NXP Employee
NXP Employee

dcbf instruction flushes both L1 and L2 caches.

Direct cache fluching via L1 control registers is not available for e5500.

L2 cache flush can be performed using L2CSR0[L2FL].


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,677 Views
hv
Contributor II

Thanks for the reply!

Would dcbst accomplish the same thing as dcbf (i.e. flushing both L1 and L2 caches)?

<http://jiveon.jivesoftware.com/mpss/c/0gA/PDcDAA/t.1rg/QZT1ok_gQ7aEHpa_HClz1Q/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

T1040 flush cache

reply from LPP<http://jiveon.jivesoftware.com/mpss/c/0gA/PDcDAA/t.1rg/QZT1ok_gQ7aEHpa_HClz1Q/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bTbcRm-2BguqOsFIlHGSwYOeV9q6IjDGpgfEN8CsLwdyYmlwYq5OM-2B1upXUGdY5w02sc-3D> in QorIQ Processors - View the full discussion<http://jiveon.jivesoftware.com/mpss/c/0gA/PDcDAA/t.1rg/QZT1ok_gQ7aEHpa_HClz1Q/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQFQji9Ev8KZJlkte9fZPI0298fgBKpIJCrctratWHxAK-2Bvf-2B7EPe6VTofdeh5HUaM-3D>

0 Kudos
Reply

5,677 Views
scottwood
NXP Employee
NXP Employee

Architecturally, dcbst will cause the cache contents to be written out, if modified, but will not guarantee that the cache block is completely removed from the cache -- though on e5500, dcbst is the same as dcbf.

It should also be noted that dcbf/dcbst only flush the specified block from the data cache, which you didn't specify.  icbi is used to invalidate a block in the instruction cache.

0 Kudos
Reply

5,676 Views
hv
Contributor II

Sorry that I wasn’t clear.

I’m working on 3 different platforms: P2041, T1040 and T2080. I need to flush caches on all 3. I think I can use dcbf to cycle through and flush all the data cache. I just want to make sure that the dcbf/dcbst will flush both L1 & L2 data caches. The T1040 has L2 backside cache so I didn’t know if I have to do something differently for that. Would dcbf take care of flushing the data cache for the platform cache too?

Thanks!

0 Kudos
Reply

5,676 Views
scottwood
NXP Employee
NXP Employee

See https://community.freescale.com/message/578951?et=watches.email.thread#578951

(why did you start two threads?)

What specifically are you trying to accomplish?  Generally dcbf is used to flush a range of addresses, not the entire cache.  If you need the entire thing flushed, why?

0 Kudos
Reply

5,676 Views
hv
Contributor II

I started 2 threads because I thought since the other thread was marked as “answered” that I would need to create a new thread for another question.

Yes, I know that dcbf is used to flush a range of addresses, not the entire cache. But I thought I can use it to cycle through the range and flush the entire cache. But that’s when I need to make sure that dcbf would flush all caches.

Why do I need the entire thing flushed, because we’re doing benchmark study and the results we got showed to show that the T1040 is much slower (2 or 3 times slower) than the T2080. We think it’s due to the cache size since the test code we used for the benchmark is a very big piece of code that we think that’s why it’s showing that much of a difference between the 2 processors. To prove/disprove that theory, we think that flushing cache cache on the processors before running the test code would give us more insights.

T1040 flush cache

reply from Scott Wood<http://jiveon.jivesoftware.com/mpss/c/mQA/PDcDAA/t.1rg/NLobBRrVTBK9jVFm3AV_9A/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSdP5biIGukMJCDP2RcupmsPmgsYXI6jS0m1mNZQcP1yOyvoqXPJhZYDmN8R-2F7Wf2U-3D> in QorIQ Processors - View the full discussion<http://jiveon.jivesoftware.com/mpss/c/mQA/PDcDAA/t.1rg/NLobBRrVTBK9jVFm3AV_9A/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bRBHj65nfOA-2FAOLmwOMEWzpe6Pz2Ey8p1mc1DKq76Htux8Ms39qJBOzCmPG5-2FWSTwA-3D>

0 Kudos
Reply