T2080 and P2041 flush cache

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 and P2041 flush cache

3,304 Views
hv
Contributor II

I learned that I can use dcbf instruction to flush both L1 and L2 caches for the T1040 (e5500).

I also need to flush caches for T2080 (e6500) and P2041 (e500mc)...would dcbf work to flush L1, L2 and platform cache for the T2080 and P2041?  does platform cache get treated differently?

Thanks!

0 Kudos
Reply
3 Replies

3,118 Views
scottwood
NXP Employee
NXP Employee

dcbf is the standard, architected mechanism to flush a cache block from all caches on all Power Architecture systems.

3,117 Views
hv
Contributor II

Yes, but if I use dcbf on the T1040, that would flush both L1 and L2 caches. Does dcbf work like that on the T2080 and P2041? That dcbf would flush both L1 and L2 caches. I’m concerned about the architectural difference among the 3 processors and that I would need to flush cache differently on all 3.

Thanks!

0 Kudos
Reply

3,117 Views
scottwood
NXP Employee
NXP Employee

dcbf affects all caches on all Power Architecture chips, including T1040, T2080, and P2041.

0 Kudos
Reply