T1040 TFTP Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1040 TFTP Problem

5,373 Views
prashanthkumarg
Contributor I

Hi,

I'm existing user of T1040 RDB bard, I'm not able to connect to the target board via Ethernet/TFTP due to his I'm unable to download the kernel/uboot loader. Request you to please support us on this, please let me know in case of any additional inputs needed.

Best regards

Prashanth

0 Kudos
Reply
6 Replies

5,171 Views
prashanthkumarg
Contributor I

Hi Val,

Thanks for your reply, I have set the u-boot parameters already as mentioned in the document. It looks their is some problem with the Ethernet communication, below are the u-boot settings used on my T1040 RDB board, I have attached the u-boot parameters and output of the TFTP commands executed. I am not able to ping the IP address itself. Please guide me on this.

Regards

Prashanth

0 Kudos
Reply

5,171 Views
valentinmovsik
Contributor I

Hi Prashanth,

I assume that 192.168.0.24 is your Linux host ip. I have a few ideas for you :

1. Did you try to work/use/donwload file from your host machine with different client machine ? I mean not from target board.

2. How many Eth ports you have on your target board ?! Did you try to use another ports ?

When your tager board is up with default img files try to run the next CLI command :

1. ifconfig -a

You should see print-out something like this :

dummy0    Link encap:Ethernet  HWaddr 06:E3:5A:23:4E:60
          BROADCAST NOARP  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

eth2      Link encap:Ethernet  HWaddr 00:04:9F:03:6E:0D
          inet addr:192.168.16.126  Bcast:192.168.16.255  Mask:255.255.255.0
          inet6 addr: fe80::204:9fff:fe03:6e0d/64 Scope:Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:28383 errors:0 dropped:28 overruns:0 frame:0
          TX packets:5381 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:8333867 (7.9 MiB)  TX bytes:781702 (763.3 KiB)
          Memory:ffe4e6000-ffe4e6fff

fm1-mac1  Link encap:Ethernet  HWaddr 00:04:9F:03:6E:0B
          BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)
          Memory:ffe4e0000-ffe4e0fff

fm1-mac3  Link encap:Ethernet  HWaddr 00:04:9F:03:6E:0C
          BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)
          Memory:ffe4e4000-ffe4e4fff

lo        Link encap:Local Loopback
          inet addr:127.0.0.1  Mask:255.0.0.0
          inet6 addr: ::1/128 Scope:Host
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

sit0      Link encap:IPv6-in-IPv4
          NOARP  MTU:1480  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

tunl0     Link encap:UNSPEC  HWaddr 00-00-00-00-B7-A8-00-00-00-00-00-00-00-00-00-00
          NOARP  MTU:1480  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

2.  dmesg | grep eth

Print-out:

[    1.858220] cpu1/4: > WARNING (FM) [CPU01, /home/val/QorIQ-SDK-V2.0-20160527-yocto/build_t1024rdb-64b/tmp/work-shared/t1024rdb-64b/kernel-source/drivers/net/ethernet/freescale/sdk_fman/Peripherals/FM/fm.c:3547 FM_Init]:
[    1.896247] fsl_mac ffe4e0000.ethernet: FMan MEMAC
[    1.899761] fsl_mac ffe4e0000.ethernet: FMan MAC address: 00:04:9f:03:6e:0b
[    1.905550] fsl_mac ffe4e4000.ethernet: FMan MEMAC
[    1.909061] fsl_mac ffe4e4000.ethernet: FMan MAC address: 00:04:9f:03:6e:0c
[    1.914850] fsl_mac ffe4e6000.ethernet: FMan MEMAC
[    1.918350] fsl_mac ffe4e6000.ethernet: FMan MAC address: 00:04:9f:03:6  e:0d
[    1.929370] fsl_dpa: fsl_dpa: Probed interface eth0
[    1.935078] fsl_dpa: fsl_dpa: Probed interface eth1
[    1.941193] fsl_dpa: fsl_dpa: Probed interface eth2
[    2.504581]      device=eth2, hwaddr=00:04:9f:03:6e:0d, ipaddr=192.168.16.126, mask=255.255.255.0, gw=192.168.16.254
[   10.894413] fsl_dpa fsl,dpaa:ethernet@0 fm1-mac1: renamed from eth0
[   10.914926] udevd[1497]: renamed network interface eth0 to fm1-mac1
[   10.919960] fsl_dpa fsl,dpaa:ethernet@2 fm1-mac3: renamed from eth1
[   10.940634] udevd[1495]: renamed network interface eth1 to fm1-mac3

The information in bold shows which eth port is actually works.

Regards,

Val

0 Kudos
Reply

5,170 Views
prashanthkumarg
Contributor I

Hi Val,

Thanks for your response. I don't have Linux image on my T1040RDB board, only option is to use U-boot. I have tried with ETH0, ETH1 and ETH2 since u-boot supports only this three Ethernet ports. I have tried with different client machines, I use windows and Linux and on both the machines the status is same. I had also tried on another machine running Windows 7 but still the status remains same. I don how to proceed further on this particular problem.

Best Regards

Prashanth

0 Kudos
Reply

5,171 Views
valentinmovsik
Contributor I

Hi Prashanth,

I'm running in T1024RDB board and when I was need to connect target to deploy kernel/uboot I was using the next doc :

http://www.nxp.com/files/soft_dev_tools/doc/support_info/QORIQ-SDK-2.0-IC-REV0.zip?fasp=1&WT_TYPE=Su...

See 4.4.13.9.1 . I hope it'll help you.

Regards,

Val

0 Kudos
Reply

5,169 Views
prashanthkumarg
Contributor I

Hi,

Can some one help me on this ?

Best regards

Prashanth

0 Kudos
Reply

5,095 Views
Wj_khi
Contributor II

Actually i have faced the same issue over t1040d4rdb board with my ubuntu host machine.  Please follow the following steps to setup the tftp at host and at board properly.

1. Stops the board boot process in uboot stage by pressing any key

2. Configure the host machine network setting (refer attached doc)

Check link status using "# ping <host ip>" . If board replied "Link is active" proceed further

3. Now setup the tftp settings on host machine. Please note that the address of tftp server location at host must be "/srv/tftpboot" (follow the steps at page 21 and 22 of attached doc)

4. Now copy all the images to server location mentioned above.

5. Execute the tftp commands from board, now it will successfully linkup the host and download the files to the board specified location.

Thanks

 

 

0 Kudos
Reply