Switch configuration for VLANs on bonding interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Switch configuration for VLANs on bonding interface

4,187 Views
mohankumarkanne
Contributor I

I'm trying to configure a T1040rdb (SDK1.7) based device to have a single LAN interface by combining fm1-gb0 and fm1-gb1 interfaces.

I chose to use bonding interface bond0 (802.3ad mode) with fm1-gb0 and fm1-gb1 as slaves. I don't see any issue with this until I configure VLANs on bond0.

It is behaving very differently from VLANs on fm1-gb0/fm1-gb1.  When I put any port on Access mode, it is always sending the packets out with vlan tag 1 (it needs to be untagged) and In Trunk mode, it is sending the untagged packets (it needs to be tagged).

Bonding Interface Configuration:

root@t1040rdb:/sys/class/net/bond0/bonding# cat mode

802.3ad 4

root@t1040rdb:/sys/class/net/bond0/bonding# cat oh_en

LAG:[CPU 0 ln 1650 fn export_oh_port_info_to_ceetm] - This oh port mapped to bond has channel:0x80a

LAG:[CPU 0 ln 1652 fn export_oh_port_info_to_ceetm] - fman_dcpid:0x0, oh_offset:0x83000, cell-index:1

LAG:[CPU 0 ln 286 fn bonding_show_oh_enable] - offline port channel:2058

1

root@t1040rdb:/sys/class/net/bond0/bonding# cat oh_needed_for_hw_distribution

fman0-oh@2

root@t1040rdb:/sys/class/net/bond0/bonding# cat slaves     

fm1-gb0 fm1-gb1

root@t1040rdb:/sys/class/net/bond0/bonding# ethtool -k bond0

Features for bond0:

rx-checksumming: off [fixed]

tx-checksumming: off

        tx-checksum-ipv4: off [fixed]

        tx-checksum-ip-generic: off

        tx-checksum-ipv6: off [fixed]

        tx-checksum-fcoe-crc: off [fixed]

        tx-checksum-sctp: off [fixed]

scatter-gather: off

        tx-scatter-gather: off

        tx-scatter-gather-fraglist: off

tcp-segmentation-offload: off

        tx-tcp-segmentation: off [requested on]

        tx-tcp-ecn-segmentation: off [requested on]

        tx-tcp6-segmentation: off [requested on]

udp-fragmentation-offload: off [fixed]

generic-segmentation-offload: off

generic-receive-offload: on

large-receive-offload: off

rx-vlan-offload: on

tx-vlan-offload: on

ntuple-filters: off [fixed]

receive-hashing: off [fixed]

highdma: on

rx-vlan-filter: on

vlan-challenged: off [fixed]

tx-lockless: on [fixed]

netns-local: off [fixed]

tx-gso-robust: off [fixed]

tx-fcoe-segmentation: off [fixed]

tx-gre-segmentation: off [fixed]

tx-udp_tnl-segmentation: off [fixed]

tx-mpls-segmentation: off [fixed]

fcoe-mtu: off [fixed]

tx-nocache-copy: off [requested on]

loopback: off [fixed]

rx-fcs: off [fixed]

rx-all: off [fixed]

tx-vlan-stag-hw-insert: off [fixed]

rx-vlan-stag-hw-parse: off [fixed]

rx-vlan-stag-filter: off [fixed]

hw-qdisc: off [fixed]

hw-accel-mq: off [fixed]

VLAN Configuration:

root@t1040rdb:~# l2switch-cfg vlan show

Printing all VLANs...

VLAN 1: 0, 1, 2, 3, 4, 5, 6, 7, 8, 9,

VLAN 10: 5, 9,  /* LAN host is connected to Port 5 */

root@t1040rdb:~# l2switch-cfg port all vlan show

Vlan port-based configuration (port - VID):

0 - VID 1

1 - VID 1

2 - VID 1

3 - VID 1

4 - VID 1

5 - VID 1      /* Configured as 1 for Trunk mode and 10  for Access Mode */

6 - VID 1

7 - VID 1

8 - VID 1

9 - VID 1

root@t1040rdb:/sys/class/net/bond0/bonding# l2switch-cfg set lag no 1 members 8 9

        LAG NO 1 members: 8 9

Packet capture on LAN device

Access Mode:

No.     Time           Source                Destination           Protocol Length Info

      2 0.018593000    54:39:68:03:e8:62     68:05:ca:15:89:32     ARP      64     192.168.2.144 is at 54:39:68:03:e8:62

Frame 2: 64 bytes on wire (512 bits), 64 bytes captured (512 bits) on interface 0

Ethernet II, Src: 54:39:68:03:e8:62 (54:39:68:03:e8:62), Dst: 68:05:ca:15:89:32 (68:05:ca:15:89:32)

    Destination: 68:05:ca:15:89:32 (68:05:ca:15:89:32)

    Source: 54:39:68:03:e8:62 (54:39:68:03:e8:62)

    Type: 802.1Q Virtual LAN (0x8100)

802.1Q Virtual LAN, PRI: 0, CFI: 0, ID: 1

    000. .... .... .... = Priority: Best Effort (default) (0)

    ...0 .... .... .... = CFI: Canonical (0)

    .... 0000 0000 0001 = ID: 1

    Type: ARP (0x0806)

    Padding: e862000000000000000000000000

    Trailer: 00000000

Address Resolution Protocol (reply)

Trunk Mode:

No.     Time           Source                Destination           Protocol Length Info

     22 83.259189000   54:39:68:03:e8:62     68:05:ca:15:89:32     ARP      60     192.168.2.144 is at 54:39:68:03:e8:62

Frame 22: 60 bytes on wire (480 bits), 60 bytes captured (480 bits) on interface 0

Ethernet II, Src: 54:39:68:03:e8:62 (54:39:68:03:e8:62), Dst: 68:05:ca:15:89:32 (68:05:ca:15:89:32)

    Destination: 68:05:ca:15:89:32 (68:05:ca:15:89:32)

    Source: 54:39:68:03:e8:62 (54:39:68:03:e8:62)

    Type: ARP (0x0806)

    Padding: e86200000000000000000000000000000000

Address Resolution Protocol (reply)

Can you guys please help me with this VLAN configuration??

Also, do you think any other better approach to achieve single interface for whole switch?? Bridging will be our last choice to go ahead with.

Thanks,

Mohan.

0 Kudos
Reply
4 Replies

3,487 Views
lunminliang
NXP Employee
NXP Employee

Hi,

1. Did you configured "Bonding driver support" in "Network device support"?

Building the Linux Kernel

Linux kernel has to be rebuilt with bonding support. In Freescale SDK this can be done by:

> bitbake -c menuconfig virtual/kernel

Select "Bonding driver support" in the "Network device support" section. Configure the driver as a module.

Build the kernel with the updated configuration and also the bonding module:

> bitbake -c deploy virtual/kernel

Installing the module

2. What are the different IP address that are being used for fm1-db0 and fm1-gb1?

3. Could you provide the commends that you run to configure the bonds? Something similar as:

> ifconfig bond0 1.0.0.2 up

> ifenslave bond0 fm1-gb0 fm1-gb1

BR

0 Kudos
Reply

3,487 Views
mohankumarkanne
Contributor I

Hi Lunmin,

Thanks for the reply,

It seems to be working now.  I was not really sure what was the problem before.

Appreciate your response.

Thanks,

Mohan.

0 Kudos
Reply

3,487 Views
lunminliang
NXP Employee
NXP Employee

Welcome, thanks for feedback, good to know it's working.

0 Kudos
Reply

3,487 Views
mohankumarkanne
Contributor I

yipingwang

Hi Yiping,

Can you please help me here.??

Please let me know if I'm heading in wrong direction here.

Thanks,

Mohan.

0 Kudos
Reply