Setting U-Boot Environment Variables with Script

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting U-Boot Environment Variables with Script

3,624 Views
smiller2
Contributor IV

Moving into a production phase of the project,  I need to make it easy from them to load U-Boot Environment variables.    Some like the MAC address change with every system.   The rest are unique to our product but the same across all devices.    I found that I could write a compiled script to enter these.  However, the script crashes on a setenv that contains multiple entries separated by semi-colons since it thinks that is a line ending.   The processor is the LS1046A.  

I found the mkenvimage command that will compile a text file list of environment variables.   However,  it requires to know the U-Boot environment size as a compile option.  When I print the environment, it lists the size as 8188.   Is that the number that I enter?      Once I compile this to a binary, then I can read it into RAM, but what command do I use to append it to the environment?    I looked by could not find any example on the web of the entire process.   My U-Boot is in QSPI flash.

Since I am also recompiling U-Boot,  can I just over-ride the defaults and add these parameters to the default settings of U-Boot?    I looked but did not find where to do this. 

 

Thanks.

 

(For anyone wanting to script U-Boot,  the mkimage  command from flexbuilder lets you do that.   I have systems with older versions of U-Boot on demo units that need to be upgraded.  I was able to compile these commands to a script with mkimage.   Since the script automates the commands, there is much less chance of someone bricking a system by entering an individual command wrong.)

 

 

0 Kudos
Reply
1 Reply

3,618 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please write MAC address variables list in variable "CONFIG_EXTRA_ENV_SETTINGS" in include/configs/ls1046a_common.h in u-boot source code, then rebuild u-boot.

0 Kudos
Reply