SPI read/write time comparison w.r.t SPI clock configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI read/write time comparison w.r.t SPI clock configuration

2,473 Views
kingshukmitra
Contributor I

I am using QorIQ P1013 processor in Linux (3.10.18), where my NVRAM Chip is connected via SPI interface.

The NVRAM Write timings calculated using Chipscope are as follows:

1 byte write time with 1 MHz SPI clock = 310 - 330 usec (approx)

1 byte write time with 10 MHz SPI clock = 260 - 280 usec (approx)

As per Chipscope calculated timing, the actual write operation are performed in correct span of time as:

For 1 MHz SPI Clock :

8 bit SPI write enable = 9 usecs (approx)

40 bit message (opcode + address + data) write = 48 usecs (approx)

For 10 MHz SPI Clock :

8 bit SPI write enable = 800 nsecs (approx)

40 bit message (opcode + address + data) write = 4 usecs (approx)

But it takes 125 - 130 usecs for wait in write completion in both 1 MHz and 10 MHz clock.

I am using standard Linux SPI driver interface where SPI write performs the following sequence of operations:

- spi_message_init

- spi_message_add_tail

- spi_sync

The spi_sync() function uses kernel task wait_for_completion() to hold the state for write completion.

As per my test results, this consumes the wait time of 125 - 130 usecs, thus adding an extra 250 - 260 usecs time in SPI write for 1 byte data.

Any suggestion or feedback to this will help in optimizing my timing requirements.

Thanks in advance,

Kingshuk

0 Kudos
Reply
2 Replies

1,858 Views
alexander_yakov
NXP Employee
NXP Employee

Instead of waiting please add another SPI command to read the status of write operation from the NVRAM Chip.

0 Kudos
Reply

1,858 Views
kingshukmitra
Contributor I

Hi,

Thank you for the response.

My NVRAM driver is implemented by using the standard SPI driver calls (see previous message) for performing read/write operations.

The spi_sync() function implementation, that waits for write completion, is part of standard SPI driver (drivers/spi/spi.c), and thus is applicable for any device connected to the SPI interface.

Refer below code snippet:

static int __spi_sync(struct spi_device *spi, struct spi_message *message, int bus_locked)

{

        DECLARE_COMPLETION_ONSTACK(done);

        int status;

        struct spi_master *master = spi->master;

        message->complete = spi_complete;

        message->context = &done;

        if (!bus_locked)

                mutex_lock(&master->bus_lock_mutex);

        status = spi_async_locked(spi, message);

        if (!bus_locked)

                mutex_unlock(&master->bus_lock_mutex);

        if (status == 0) {

                wait_for_completion(&done);

                status = message->status;

        }

        message->context = NULL;

        return status;

}

Please tell me how the implementation specific to NVRAM write completion can be achieved using the Linux SPI driver calls.

Thanks again,

Kingshuk

0 Kudos
Reply